electronica 2022 behind the scenes and what the industrial live stream didn’t show you!

mi factory automation hero

Today, ST held a new live stream on industrial applications at electronica 2022. It featured partners demonstrating their solutions to critical challenges, experts explaining how to address the energy crises we face, and a presentation on how car batteries will power our homes thanks to a European effort. However, that’s only a fraction of what we are presenting at the ST Booth here at electronica 2022. Hence, to surprise our blog readers, here’s a demo that didn’t make it to the live stream.

MI factory rail and robot arm

The root arm and factory automation demo from MI.
The root arm and factory automation demo from MI.

The presentation introduces a robot arm that loads a cassette containing wafers onto a conveyor belt and then retrieves it at the end of the line. It simulates a sensitive asset traveling within a site. The demo itself reflects actual machines already deployed in ST factories, and a map displays the real two-kilometer trip a similar asset takes within our operations.

On the demo, the cassette crosses checkpoints, each equipped with a display highlighting critical industrial features like condition monitoring, asset tracking, predictive maintenance, and more. This demo is, therefore, highly symbolic because it embodies all the concepts we covered on Day 2 at electronica into one application. Companies wishing to work on similar applications can start using the STEVAL-ASTRA1B development board, which includes an STM32WB and an STM32WL.

Scroll to Top